Trigger Level

This is an analyzer sequence parameter which specifies the input power level (in dBm) to the test set which is required to trigger the acquisition (provided that the Input Trigger Type parameter has been set to "VIDeo").

There is no dropdown list for this field; it is necessary to enter a suitable value, or accept the default value of -20 dBm.